Wearables

Xadow appearing as storage device on linux

I got my Xadow yesterday and am having fits trying to get it to work. I _think_ I have the arduino IDE configured as instructed, but
a) I don't see any serial port created when I connect the Xadow to the system
b) the IDE trys to use the AVR109 Boot Loader which fails

When I use the mbed online IDE I can see the device as flash storage. It has one file - firmware.bin. I can remove this file and replace it with my .bin created by mbed. I can unmount the device and remount it and the file is fine. When I reset the Xadow or remove power, my image disappears and the firmware.bin returns.
Joe KirbyDec 18,2015 22:40 PMAdd Comment

Comment

Popular Topics