Wearables

Xadow GPS v2 Returning 0 for both LAT and Long

Hello,

When I run the gps_test example I am getting the following output

GPS UTC:16-2-28 13:20:55
GPS status is V
GPS latitude is -:0.000000
GPS longitude is -:0.000000
GPS speed is 0.000000
GPS course is 0.000000
GPS position fix is 0
GPS sate used is 0
GPS altitude is 0.000000
GPS mode is A
GPS mode2 is 1
GPS UTC:16-2-28 13:20:56
GPS status is V
GPS latitude is -:0.000000
GPS longitude is -:0.000000
GPS speed is 0.000000
GPS course is 0.000000
GPS position fix is 0
GPS sate used is 0
GPS altitude is 0.000000
GPS mode is A
GPS mode2 is 1

can anyone please help?

Thanks
bleusrFeb 28,2016 21:29 PMAdd Comment

Comment

Popular Topics