wio

Wio Won't connect anymore? Seems to be useless now

Hello, I have been having problems with my Wio connecting after being successful the first time. In order to attempt to fix the issue I removed the node via the API and then via the app afterwards. Now that I have done that I can no longer get my Wio node to connect when I add it back. I have tried adding it through the App, that didn't work (firmware wouldn't download and it wouldn't show up online). I also tried adding it via the API using the same name in case that was the issue but that did not fix the problem. I am now stuck with a Wio node that doesn't seem to work at all, how can I fix this?

dandmendelsohnMar 12,2018 20:18 PMAdd Comment

Comment

Popular Topics