Water Sensor Project

62910Published On Sep 21,2009 12:19 PMshare0
Connecting a water sensor to an Arduino is a great way to detect a leak, spill, flood, rain etc. It can be used to detect the presence, level, volume and/or the absence of water. While this could be used to remind you to water your plants, there is a better Grove sensor for that. The sensor has an array of exposed traces which will read LOW when water is detected. In this tutorial, we will connect the Water Sensor to Digital Pin 8 on the Arduino, and will enlist the very handy Grove Piezo buzzer and an LED to help identify when the Water sensor comes into contact with a source of water.

Step by Step Introduction

Comment

ArduinoBasics
Followers0
Projects5
Components
4xAA Battery Holder
$1.50 Add To Cart
Grove - Universal 4 Pin 20cm Unbuckled Cable (5 PCs Pack)
$2.90 Add To Cart
Grove - Buzzer
$1.90 Add To Cart
Grove - Base Shield
$8.90 Add To Cart
Grove - Water Sensor
$2.90 Add To Cart
Add All To Cart
Related Recipes
Popular Recipes