Use Lora shield and RPi to build a LoRaWAN gateway

76761Published On Jul 03,2016 14:33 PMshare1

Over here,we will use the Lora Shileld,MEGA2560 and Raspberry Pi to build a single channel LoRaWAN gateway.

LoRa Technology is a wireless modulation for long-range, low-power, low-data-rate applications. By achieving a range of more than 15 kilometers in a suburban environment and more than 2 kilometers in a dense urban environment, LoRa technology solutions target multiple application domains, such as Internet-of-Things (IoT), metering, security, and machine-to-machine (M2M).

 This single channel LoRaWAN gateway is a proof-of-concept implementation,that can be used for development and node testing. It is not a replacement for a real multi channel/multi SF gateway! It supports some LoRaWAN features, but due to its static nature (single channel) it is not fullyLoRaWAN compatible (and will never be)
By default it works with the TTN backend, for testing and development.
 Refer to the summary of Thomas

Step 1: Hardwares

Step 2: A brief introduction of the Dragino Lora Shield

Step 3: Network structure

Step 4: Create an Account on TTN network

Step 5: Create a Gateway on TTN network

Step 6: Build a single channel LoRaWAN gateway

Step 7: Connect the Lora Shield and MEGA 2560,upload the skt

Step 8: Conclusion

Comment

Berlina
Followers20
Projects79
Components
Dragino LoRa Shield - support 868M frequency
$21.00 Add To Cart
Related Recipes
Popular Recipes