Use LinkNode to Control a Servo through LinkSpriteIO

15090Published On Nov 21,2016 16:45 PMshare0

LinkSpriteIO provides an IOT server platform to control things. LinkNode is a WiFi board that is compatible with Arduino programming.  In this tutorial, we show how to program the LinkSpriteIO and LinkNode so that we can remotely control the servo that is attached to LinkNode.

This tutorial uses the following parts:

Wiring diagram:

  • Servo VCC (Red wire)     -> LinkNode D1 5V
  • Servo GND ( gray wire )   -> LinkNode D1 GND
  • Servo Signal (yellow wire) -> LinkNode D1 GPIO15 ( Arduino-D10 )

step1

Comment

firstname lastname
Followers0
Projects29
Related Recipes
Popular Recipes