Use LCD.print() to display information on I2C_LCD

25721Published On Jun 05,2016 12:37 PMshare1
I2C_LCD is an easy-to-use open source display module, It can make display easier. Using it can reduce the difficulty of make something, so that makers can focus on the core of the work.
There is Arduino library for I2C_LCD, user just need a few lines of the code can achieve complex graphics and text display features.

This is a demo project for how to use LCD.print() function to display what you want on I2C_LCD, and how to print characters on I2C LCD by computer serial monitor.

Download the files what we need.

Install the Arduino library for I2C_LCD.

Hardware Connection.

To use LCD.print() function as Serial.print().

Coding and upload.

Test and enjoy.

Comment

Joney
Followers0
Projects6
Components
I2C_LCD(With universal Grove cable)
$17.90 Add To Cart
I2C_LCD(With conversion Grove cable)
$17.90 Add To Cart
Seeeduino Lotus - ATMega328 Board with Grove Interface
$17.50 Add To Cart
Add All To Cart
Related Recipes
Popular Recipes