The Talking Breathalyzer

54401Published On Sep 14,2008 16:57 PMshare1
*** A fully assembled version of the Talking Breathalyzer is available here from Seeedstudio and additional info at http://talkingbreathalyzer.com***

Video of the Talking Breathalyzer in Action:


More detail on the Talking Breathalyzer:




A customizable Breathalyzer that talks and tells you how much you’ve had to drink. It’s also open source and can easily be modified with your own text on the LCD screen and audio MP3 files.

When tethered to a PC with a USB cable, it has additional features including character animations, Breathalyzer Tweets, text to speech, weather and stock read-outs, and a Photobooth feature.

The Talking Breathalyzer is not a professional Breathalyzer and should be used for Amusement Purposes Only.

Part List

Seeeduinoor Arduino - $25
Seeed Music Shield - $27.50
Seeed Twig Alcohol Sensor - $7.90
Seeed Twig Serial LCD - $13.90
Seeed Twig Cables - $4.90
2 GB MicroSD card (cards larger than 2GB will not work) - $7
Protoboard
10k Potentiometer
4 Momentary Switches
1 Off/On Switch (for power)
5 10k Resistors
1 Toggle Switch
Enclosure of your Choice
LIPO Battery - $23
LIPO Rider - $9.50
Talking Breathalyzer Software - Free
Head Phones
Mini USB Cable
USB Charger
Solar Panel Optional
Speaker Amp and Speaker Optional

*** A fully assembled version of the Talking Breathalyzer is available here from Seeedstudio and additional info at http://talkingbreathalyzer.com***

Step 1 Schematic and Assembly

Step 2 Using the Breathalyzer in Portable Mode

Step 3 Using the Breathalyzer USB Tethered to a PC (PC Mode)

Step 4 How to Switch from Portable Mode to PC Mode and Vice Versa

Step 5 Customizing the Breathalyzer in Portable Mode - Arduino Code Walk Through

Step 6 Adding Custom Functions in Portable Mode

Step 7 The Source Code for PC Mode - Adobe Flash Action Script 3.0

Step 8 Software Installation and Manual

Step 9 Alternate Case Installation

Comment

xieliangliang
Followers0
Projects29
Components
The Talking Breathalyzer (Assembled)
$199.00 Add To Cart
Seeeduino V3.0 (Atmega 328P)
$9.90 Add To Cart
Music Shield
$27.50 Add To Cart
Grove - Alcohol Sensor
$7.90 Add To Cart
Grove - Serial LCD
$13.90 Add To Cart
Grove - Universal 4 Pin 20cm Cable (5 PCs Pack)
$2.90 Add To Cart
SanDisk microSD™ Card 2GB
$6.90 Add To Cart
Li-po Rider
$9.50 Add To Cart
Add All To Cart
Related Recipes
Popular Recipes