The Internet Of Led Wall!

54841Published On May 24,2016 10:38 AMshare1

Here is the lovely tiny LED wall I made with Wio nodes. Every one can control it through the internet.


There are 30 LED bars on the board, each bar has ten led. Every one in every where can control every bar he/she likes with the API of Wio link.

 

Here is the step to implement the Internet Of Led Wall

1.Use the laser cutting to make a wood board to fix every le

2.configure every I/O of the wio link or wio node.There are

3.Connect the led bar to wio node grove interface with grove

4.Choose the number of the led you want to control

5.Then you will see the amazing effect of the wio link

Comment

James@Seeed.cc
Followers7
Projects8
Components
Wio Node
$9.90 Add To Cart
Grove LED Bar v2.0
$3.90 Add To Cart
Add All To Cart
Related Recipes
Popular Recipes