features:-control the water in the tank (if to low switch all water tools off)-control the humidity (if over 70% switch foger off )-control light (switch light on at 6h00 and off at 23h00)-control Temp (if under 30°C switch heaters on if over 35°C switch off)-control Heater (if temp over 45°C switch off under 30°C switch on)-control rain (set the rain interval to 2h raining delay to 2 min)-control LCD (2 lcd displays to show infos)-SD Data logger-html display page (show infos in Auto and in Manu mode switch different outputs )-change the stettings over html pagein the next weeks i want to post the complet project with instruction and more infos my new version is stable (works fine under internet explorer)thx