Running Mosquitto (MQTT broker) on Raspberry Pi

36432Published On Jul 29,2016 13:56 PMshare2

Start with a fresh new Pi (B+):

  • Put the latest Raspbian image on an SD
  • Raspi-config: expand filesystem, enable SPI, set timezone, change password
  • Optional: set up wifi, static IP, and reboot
  • Run rpi-update, apt-get update, apt-get upgrade
  • Reboot and switch to using terminal (instead of directly connected screen & keyboard)


          This recipe is orginally written by  Ivegotatheory

Install Mosquitto

Test Mosquitto

Troubleshooting:

Comment

James
Followers20
Projects98
Related Recipes
Popular Recipes