Push to data.sparkfun.com from an Intel Edison with Node.js

24600Published On Jun 19,2016 19:46 PMshare0

The Intel Edison is really great at doing a lot of things, but one of the things that I was most excited about was its ability to use Node.JS to interact with objects IRL. As a front-end dev and a maker, I'm just trying to keep Atwood's Law true, haha!

The Intel Edison comes with wi-fi ready to roll after minimal configuration, and it's really easy to add Node.js to the platform with Intel's Yocto image. Once we get that up and running, I'm going to show you how to use Node to push data to a stream on data.sparkfun.com.

Step 1: What We're Actually Building

Step 2: Configure Your Edison and Load the Yocto Image

Step 3: Hook Up Your Sensor

Step 4: Create a Feed on data.sparkfun.com

Step 5: Set Up Your Dev Environment

Step 6: Write Your Code

Step 7: Run Your Code

Comment

Berlina
Followers20
Projects79
Components
Intel Galileo
$98.00 Add To Cart
Grove Starter Kit Plus - IoT Edison
$79.00 Add To Cart
Add All To Cart
Related Recipes
Popular Recipes