esp8266Arduino

NEED HELP - INSTALLING SEEEDUNIO WITH ESP8266

Hi everyone,

I am a newbie and facing this issue.

i using Seeedunio v4.2, Base Shield and ESP8266.

I had tuned the volt to 3.3v and using jumper cable to connect between ESP8266 and base shield as you can see from the picture.

I can upload without issues. the only problem is 
when i use putty to access, i do connect but i cannot able to send AT command to do further testing.

Can anyone enlightened me with some light?

i am not sure what i doing is correct


Thank you.

michaellinlwOct 16,2016 10:26 AMAdd Comment

Comment

Popular Topics