Missed Call Notifier Using ESP8266

67460Published On Mar 05,2010 00:38 AMshare0
One of the first projects I had created when I started my journey into electronics was a missed call notifier (http://dushyant.ahuja.ws/2013/11/physical-android-notifier/). Unfortunately it used bluetooth and a workaround using Tasker, S4LA and Python to work, which stopped working some time about a year ago. I think probably due to an android upgrade. Don't know, didn't really bother to check again.However, I still wanted one, just to ensure that I see if there's any missed call, even if my phone is either in my bag, or in the other room. Recently I had bought a couple of ESP8266 modules (ESP-01) and thought this might be a good first project. Didn't need many GPIOs, and wifi would be easier to work than bluetooth (as Tasker can directly access web pages).

Step by Step Introduction

Comment

dushu
Followers1
Projects7
Components
Europe Standard USB Wall Power Supply 5VDC 2.1A - CE Intertek GS
$6.95 Add To Cart
USB To Uart 5V/3V3
$7.95 Add To Cart
WiFi Serial Transceiver Module w/ ESP8266
$6.95 Add To Cart
Add All To Cart
Related Recipes
Popular Recipes