Inside-Outside Weather Station

22543Published On Aug 04,2017 15:52 PMshare3

This project is made by Carmelito Andrade on hackster.io, shared on #SeeedSummerShare.

This is a great weekend IoT project which uses the BeagleBone Green to display Temperature Humidity inside and outside your home and more..

Here a quick video demo, of the features implement as part of the project.


●Display Temperature and Humidity inside your home using the Grove -Temperature and Humidity sensor -pro version

●Get the Temperature and Humidity of you city to display on Grove LCD using http://openweathermap.org/ 

●Get Weather conditions to display, so that you can plan what to wear or if you need to carry you umbrella before you head out in the morning.

●Post the temperature and humidity values  to dweet.io from a data collection endpoint

●Create awesome dashboards using freeboard.io

3D Print the Case for BBG and Sensors

Solder Bread-Boarding Wire to the Grove Connectors

Install Python Library for the Temperature and Humidity sens

Install Python Libraries & get OpenWeathermap API Key

Getting Weather of your City

Complete the Circuit

Run the Python Program on start of BBG

Create Dashboards on Freeboard.io

CODE

Comment

E1even
Followers0
Projects4
Related Recipes
Popular Recipes