Grove Starter Kit With LinkIt One

19563Published On May 18,2016 16:57 PMshare3

When I started with IoT I was all confused about electronics stuffs, resistors and circuits, then I got Seeed Studio’s Grove Starter Kit plus. With this we have to just plug the sensor modules instead of managing it through soldering or breadboard. So let us see how easily we can get started with Internet of Things with Grove Starter Kit without worrying about electronic component and circuits. The Grove Starter Kit is a complete development kit that consists of a collection of sensors, actuators and shields. It is a hardware and software solution to help you explore the IoT space and create innovative projects. The Grove Starter Kit is a better choice because: It accelerates development and testing with IoT. The Grove shield and sensors has 4 pin connectors that allow us to plug in the sensor with ease rather than managing circuits and sensors using breadboard. The Grove shield has been tested as compatible with Windows by the Windows IoT team. There is a huge variety of sensor modules available with Seed Studio. If you are new to IoT, the Seed Studio Grove Starter Kit will help you to easily get started with development since you need not worry about circuits and other electronics stuff. With Grove shield and sensor modules you can easily create anything without worrying about electronic components much. There is no need to manage sensors using soldering or a breadboard. This article will guide you about how to set up and get running with the Grove Starter Kit plus and LinkIt One. The booklet contains instructions about basic sketches with Grove Starter Kit Plus.

For more information, please head over to the original  written by  opoojabaraskar.

Adding SketchBook to Arduino IDE

Making Connections

Adding Grove Base Shield

Displaying Hello world on LCD

code

Comment

molly
Followers13
Projects25
Components
LinkIt ONE
$59.00 Add To Cart
Grove - Starter Kit
$39.00 Add To Cart
Add All To Cart
Related Recipes
Popular Recipes