Flappy Duino

33172Published On May 14,2016 18:18 PMshare2
FlappyBird is no longer on the App Store. For sometime I missed it.I had this project last year (2014, when FlappyBird is still hot) as part of the"Arduino Day"event. The idea is to recreate the game using simple hardware, and also change the gameplay by involving more real action. For real action the player has to"flap"his/her hand to fly the bird. The"flapping"action is detected by a distance sensor. It continuously measures hand position, the data is then converted to"moving close"or"moving away"actions, so as to determine the up/down acceleration of the bird.

Step by Step Introduction

Comment

Baoshi Zhu
Followers0
Projects2
Components
Arduino Pro Mini 328 - 5V/16MHz
$9.95 Add To Cart
Grove - 80cm Infrared Proximity Sensor
$13.90 Add To Cart
Add All To Cart
Related Recipes
Popular Recipes