Esp8266 firmware update

31050Published On Jul 03,2016 15:21 PMshare0

WP_20150311_001 (2).jpg

The ESP8266 module is a cheap Wireless module.It has SOC(system on chip) that can handle TCP protocols.By default, these modules come with an AT command processor and can act as a serial to WiFi bridge. There is lots of info on the web about this module.

I got 3 of the ESP8266 for my home automation project, initially the module was working perfect.

butaccidentlyiuploadedwrong files and my esp8266 stopped working after then the serial port was giving me random garbage values,soi tried myself to solve this problem.


Step 1: Find an esp8266 flasher.

Step 2: Find proper ESP8266 firmware files or bin files.

Step 3: Connecting ESP to Flash mode

Step 4: Uploading Firmware

Step 5: Using esp flash download toll v0.9.3.1

Step 6: Program esp using esplorer

Step 7: Troubleshooting

Comment

Berlina
Followers20
Projects79
Components
WiFi Serial Transceiver Module w/ ESP8266
$6.95 Add To Cart
Related Recipes
Popular Recipes