dhcpwirelessesp8266

ESP8266

Hi,


I am using"Grove - UART Wi-Fi"module to connect to  WIFI network. I set the board to use DHCP to get an IP address.

Usually a conventional PC or cellphone includes its hostname inside DHCP request packet. But, the aforementioned module does not do that.  

Is there a way to change its firmware to set a hostname and use it for DHCP? Where should I start from? It can be either hard coded or done through AT commands.


Regards


 

h.ahmadi86Sep 23,2017 03:50 AMAdd Comment

Comment

Popular Topics