Blinds Automation using LinkIt ONE

13670Published On Jun 26,2016 08:58 AMshare0

IMG_9498.JPGIMG_9530.JPG

Automatingyou blinds, is a great weekend project, you can put together usingMediatek LinkIt ONE platform and 3D printed parts for which the STL files are attached in step 2.

To rotate the blind wand/rod we will use a continuos rotation servo. And the movement of the blinds will be triggered from a Wi-Fi web app hosted on the LinkIt one as part of the Arduino code, which you can access using your phone,tablet or computer.


Step 1: Things you'll need to complete the build

Step 2: 3D print STL files attached

Step 3: Putting the 3D Printed parts and electronic together

Step 4: Upload the Arduino Code

Step 5: Adding the circuit to the blinds

Comment

Berlina
Followers20
Projects79
Components
LinkIt ONE
$59.00 Add To Cart
Related Recipes
Popular Recipes