wio

Adafruit Feather HUZZAH ESP8266 Battery ISSUES

Hi,

I recently bought an adafruit feather HUZZAH ESP8266 and I found a 3.7 v 150 mAh LiPo battery I had lying around.

I plugged the battery in to the onboard connector and I got a small pop and the board heated up and gave off a bit of smoke.

I immediately unplugged the battery from the connector and tested the Blink sketch through the USB cable.

The sketch worked and i saw no visible problems on the board. 

I was just wondering if the board would still work fine because I have no use for the battery connector or if I need to get a replacement.

What should I do?

Please help.

Thanks!

I didn't find the right solution from the Internet.


References: https://forums.adafruit.com/viewtopic.php?f=24&t=127012


Animated medical business video




explainervideo6Dec 16,2017 19:47 PMAdd Comment

Comment

Popular Topics