ADC with TLC1543: Raspberry Pi B to Arduino Adapter HAT for Raspberry Pi B

13030Published On Aug 10,2016 14:28 PMshare0

Here we discuss how to use the ADC chipset TLC1543 with Raspberry Pi B+.

1. Configure A0 pin to be ADC pin.

1) Install libraries as shown in steps shown here.

2) Set the jumpers to select the reference voltages:

  • When REF is connected to 5V, the reference voltage of ADC is 5V (by default).
  • When REF is connected to 3V3, the reference voltage of ADC is 3.3V.
  • Note: only one at once.

step 1

step 2

Comment

firstname lastname
Followers0
Projects29
Related Recipes
Popular Recipes