3.2.2.ADC

8580Published On Oct 21,2016 18:47 PMshare0

#includevoidsetup() {//Initialize serial with baudrate setting, the default config is SERIAL_8N1  int rate = 115200;  Serial.begin(rate);  //you will see the string on the terminal  Serial.println("Serial begin:");}void loop() {  //if you type the character in the terminal, available() will return the size you typed  if (Serial.available() > 0) {    // read the incoming byte:    char thisByte = Serial.read();    //print it on the terminal with DEC format    Serial.print("I received:");    Serial.println(thisByte, DEC);  }  delay(200);}

Step 1

Step 2

Comment

firstname lastname
Followers0
Projects29
Related Recipes
Popular Recipes