Product FAQGroverpiarduinoShieldplatecompatiblerespberry pirs pi

[FAQ]yoshg asked about Arduipi

i seen that the arduipi becomes the slave to the raspberry pi in the case of the SPI. my question here is; with the arduipi if its taking up the CS pin to the RPI can you remap RPI to use other pins as slaves? also then if you were to use SPI from the
https://www.seeedstudio.com/Arduipi-p-1609.html

yoshgOct 19,2016 20:24 PMAdd Comment

Comment

Popular Topics