Product FAQbatterylipopowerarduinoenergyportable

[FAQ]seeedstudio asked about LiPo Rider Pro

The wiki says"2 x USB ports let you program your kit while charging your Lithium battery"but when I have a Seeeduino v4.0 plugged into the LiPo Rider Pro, and the LiPo Rider Pro is plugged into my PC, the Seeeduino is not detected as an attached serial device and the Arduino IDE does not detect it. Is there something else I need to do, such as add resistors in the R25-R28, to get USB pass-thru on the LiPo Rider Pro?


/LiPo-Rider-Pro-p-992.html
Chris O'HalloranOct 27,2018 19:11 PMAdd Comment

Comment

Popular Topics