Product FAQgalileoarduinoIoTwirelessreader125khzrfidcredit carduem4100Grovelinkit onedoor access

[FAQ]progettazione asked about Grove - 125KHz RFID Reader

dear SirI have a problem with a reader application, because usually the client enters inside and put the RFID tag inside a box in proximity of the antenna, but if the tag is always in the same position respect the antenna, the reader reads it only the first time. So becouse I have to check continously the presence of the tag to solve the issue I have to disconnect the power supply and periodically reapply to the reader.


https://www.seeedstudio.com/Grove---125KHz-RFID-Reader-p-1008.html
progettazioneMay 08,2017 01:19 AMAdd Comment

Comment

Popular Topics