Product FAQlong rangearduino434mhzwirelessserialrangeCC1101Communicationrf

[FAQ]orders asked about 433Mhz Wireless Serial Transceiver Module - 1 Kilometer

Hi, I have used this module in my product design, where one unit communicates to multiple sensors. I wished that this module had an addressing technique which you could enable/ disable and set the address using AT commands. At this stage I have to do addressing in the source code, all modules outputs the transmitted information as long as they are in the same channel. Is there a possibility of updating the firmware to incorporate addressing if needed?


https://www.seeedstudio.com/433Mhz-Wireless-Serial-Transceiver-Module---1-Kilometer-p-1733.html
ordersNov 14,2017 15:53 PMAdd Comment

Comment

Popular Topics