Product FAQ

[FAQ]nive asked about Seeedstudio Grove - TF Mini LiDAR

Hi, a question about enter /exit configurationmode.The sensor is working fine. I got confused when trying to set parameters (table 8 in the Productmanual)First command"Enter Config mode", then actual command, example change Unit of distance to mm, and finally"Exit Config mode".Only way I got it to work was by just sending the actual command 42 57 02 00 00 00 00 1A.Nothing more.Have I misunderstood something ? Grove - TF -Mini Lidar 114991434 Sed Studio MOA 180403012 05/11/18


/Seeedstudio-Grove---TF-Mini-LiDAR-p-2996.html
niveSep 09,2018 04:04 AMAdd Comment

Comment

Popular Topics