Product FAQLCD

[FAQ]markaaronpeacock asked about 10.1 Inch LCD Display - 1366x768 HDMI&VGA&NTSC&PAL

I have one, now how do I connect the female header with the white dot, it's smaller than the male header, in terms of pin count! is there a wiring diagram or"how-to-connect"anywhere for this driver board and screen combo? i bought one from mouser but it's a seeed studio 10.1 inch lcd with board 2AV-1VGA-1HDMI-TTL-50PIN-LVDS-ACC that has an HDMI, a vga, and an s-video out. How do I connect it via HDMI?


/10.1-Inch-LCD-Display---1366x768-HDMI&VGA&NTSC&PAL-p-1586.html
markaaronpeacockDec 02,2018 19:24 PMAdd Comment

Comment

Popular Topics