Product FAQ

[FAQ]m.travan asked about Serial CAN-BUS Module based on MCP2551 and MCP2515

No one knows why CAN Bus Serial does not work with AT commands from a serial port of MKR Zero Arduino? Excluding obviously the library that is not provided for the SAMD.


/Serial-CAN-BUS-Module-based-on-MCP2551-and-MCP2515-p-2924.html
m.travanNov 13,2018 00:46 AMAdd Comment

Comment

Popular Topics