Product FAQ

[FAQ]joel.candia.p asked about Grove - LoRa Radio 868MHz

hello I tell you that I have two Grove LoRa Radio 868MHz modules, which I want to make a point-to-point communication between the two radios using 2 Arduino Uno boards, to connect the radio to arduino I also bought 2 Base Grove Shield V2 and I used the code of examples that the Lora Grove library brings to the client and server. I would like to know if you can help me since entering the codes does not work.


/Grove---LoRa-Radio-868MHz-p-2776.html
joel.candia.pNov 06,2018 06:12 AMAdd Comment

Comment

Popular Topics