Product FAQkitreaderCommunicationwirelessrf

[FAQ]danmarcado asked about 2KM Long Range RF link kits w/ encoder and decoder

Hello, I have problems with this module. First of all, when I try to use the receiver with 9V it fail and you can`t use it anymore(2 units failed in the same way). And when I was using 9 V for the transmitter and 5V for the receiver the range was 60 me
https://www.seeedstudio.com/2KM-Long-Range--RF-link-kits-w-encoder-and-decoder-p-321.html

danmarcadoOct 19,2016 19:48 PMAdd Comment

Comment

Popular Topics