Product FAQ

[FAQ]b-projekte asked about Serial CAN-BUS Module based on MCP2551 and MCP2515

Hi, I need to connect some Batteryes with UART Communication with a CAN System. Therefore I have to translate the UART Battery informations such as state of charge, designed capacity, … to a CAN protocol (all CAN and UART signals known). As your board has a Atmega processor onboard it could theoretically do that without any external processors. Is there a way to get access to the processor for such an applications?


https://www.seeedstudio.com/Serial-CAN-BUS-Module-based-on-MCP2551-and-MCP2515-p-2924.html
b-projekteMay 09,2018 01:05 AMAdd Comment

Comment

Popular Topics