Product FAQ

[FAQ]ashish.sajwan91 asked about Serial CAN-BUS Module based on MCP2551 and MCP2515

I intend to use this module like a bidirectional RS 232 to CAN converter, using a UART to RS232 level shifter. RS 232 end will connect to a device and CAN to a PCI card on my PC. Will this work? If yes, how do I set baud rates, termination, etc. for the serial and CAN?


https://www.seeedstudio.com/Serial-CAN-BUS-Module-based-on-MCP2551-and-MCP2515-p-2924.html
ashish.sajwan91Sep 01,2017 05:34 AMAdd Comment

Comment

Popular Topics