Product FAQrespeakerrespeaker2.0respeaker core v2.0respeaker coresmart echo

[FAQ]andreandreoli93 asked about ReSpeaker Core v2.0

Is the device recognized as an input audio device if connected via USB to a PC running Debian? Can it be used with the Snips platform?


https://www.seeedstudio.com/ReSpeaker-Core-v2.0-p-3039.html
andreandreoli93Apr 23,2018 18:00 PMAdd Comment

Comment

Popular Topics