Product FAQcurrent changewirearduinoenviromentIoTraspberry pielectricitygalileoGrovecurrentSensorlinkit one

[FAQ]Stanley Caramoy asked about Grove - Electricity Sensor

I'm using this sensor to detect current. But something is wrong. If my device goes on, it takes 150mA, if not then 0mA. I can measure it using AV-Meter. If I use this sensor with the demo code, it shows me only the changes (0mA then 150mA then back to
https://www.seeedstudio.com/Grove---Electricity-Sensor-p-777.html

Stanley CaramoyOct 19,2016 19:56 PMAdd Comment

Comment

Popular Topics