Product FAQ

[FAQ]Skinner.David asked about Serial CAN-BUS Module based on MCP2551 and MCP2515

I can't seem to get this module to work with extended frames? I've set the EXT frame bit to"1"but the receiving CAN module doesn't output any serial data? If I set the EXT frame bit back to"0"then everything works fine again. Any ideas what would cause this?


https://www.seeedstudio.com/Serial-CAN-BUS-Module-based-on-MCP2551-and-MCP2515-p-2924.html
Skinner.DavidApr 04,2018 17:42 PMAdd Comment

Comment

Popular Topics