Product FAQLED

[FAQ]SImon asked about Rainbowduino LED driver platform - Atmega 328

Hi, is it normal that the output current of the led drivers ist just about 1.65 mA when I write commands like"Rb.setPixelXY(0,0,255,255,255)? I use the Rainbowduino v.3.0 with the firmware from the wiki page and some RGB LEDs with a current of 20 mA.
https://www.seeedstudio.com/Rainbowduino-LED-driver-platform---Atmega-328-p-371.html

SImon HellerOct 19,2016 19:48 PMAdd Comment

Comment

Popular Topics