Product FAQ

[FAQ]Pallav Agrawal asked about Music Shield

The shield is working fine with the musicPlayAll code i.e the one which uses the inbuilt SD library of arduino.while using the same setup if i upload the MusicShieldNewSDLib codes using the FAT 16 LIBRARY then it shows"Fat16::init
error: open file
https://www.seeedstudio.com/Music-Shield-p-642.html

Pallav AgrawalOct 19,2016 19:51 PMAdd Comment

Comment

Popular Topics