Product FAQ

[FAQ]Nicholas asked about Grove - Base Shield

Because the 6 and 8 pin connectors that connect this shield are short, when it is placed above ethernet shields the contacts can short out on the ethernet port. I tend to standardise a height between shields as 15mm with nylon spacers and this clears t
https://www.seeedstudio.com/Grove---Base-Shield-p-754.html

Nicholas GordonOct 19,2016 19:55 PMAdd Comment

Comment

Popular Topics