Product FAQ

[FAQ]Mitchel Daams asked about Serial CAN-BUS Module based on MCP2551 and MCP2515

Could you also create a version with 2 canbus controllers and a ATMEGA328 that is programmable throuh the Arduino IDE ?That would be killer as you could build filters, translators, 2 ways monitors and the like. Something I'm still looking for.Add a K-LINE/LIN tranceiver and you got the ultimate automotive hacking device


https://www.seeedstudio.com/Serial-CAN-BUS-Module-based-on-MCP2551-and-MCP2515-p-2924.html
Mitchel DaamsSep 15,2017 04:42 AMAdd Comment

Comment

Popular Topics