Product FAQkeyswitchbuttonGroveraspberry pipinterfacearduinopushIoT

[FAQ]Megha Dhingra asked about Grove - Button(P)

Is the Grove Cable included with the button? Also, since this is only a momentary button (it automatically unreleases after being pressed) is there any way I can make a buzzer beep for 20 seconds if the button only pressed for a moment...or should I use another product instead of the button. Thanks!


https://www.seeedstudio.com/Grove---Button(P)-p-1243.html
Megha DhingraJul 31,2017 16:35 PMAdd Comment

Comment

Popular Topics