Product FAQcarmotor4wdmechanicrobotgear

[FAQ]Kristoffer asked about L298 Dual H-Bridge Motor Driver

Hi

Can't get it to work with a Netduino.
I'm using a power supply that outputs 24V DC 5.0A connected to VMS and GND ad the power Led lights fine.

Settings from Netduino:
EA to 3.3V
I2 high
I1 low

Result is that one of th
https://www.seeedstudio.com/L298-Dual-H-Bridge-Motor-Driver-p-284.html

Kristoffer OlssonOct 19,2016 19:49 PMAdd Comment

Comment

Popular Topics