Product FAQShieldtftdisplayLCDarduinotouchscreen

[FAQ]Johannes Glaser asked about 2.8'' TFT Touch Shield V2.0

Hi, is it correct that the '2.8"TFT Touch Shield V2.0' is using the following pins of the Arduino Uno r3 or are there any more (like ICSP) pins used? Pins: D4, D5, D6, D7, D10, D11, D12, D13, A0, A1, A2 and A3. Kind regards, Johannes...


https://www.seeedstudio.com/2.8-TFT-Touch-Shield-V2.0-p-1286.html
Johannes GlaserOct 19,2016 20:14 PMAdd Comment

Comment

Popular Topics