Product FAQwizfi210wpaWifiwirelessraspberry piShieldwizfiwepudp tcp/ip dhcp arp dns http/httpsarduino802.11

[FAQ]Jim asked about WizFi Shield

Why not connect the UART through a switch do the user can enable or disable it as they prefer?

Finally, you might be better off driving your voltage regulators from Vin instead of +5V on the Arduino board. Vin should have greater current availabl
https://www.seeedstudio.com/WizFi-Shield-p-1403.html

Jim ArcherOct 19,2016 20:20 PMAdd Comment

Comment

Popular Topics