Product FAQ80cmarduinoinfraredsecurityIoTSensorproximitygalileomovementGrovewirelesslinkit one

[FAQ]Jay asked about Grove - 80cm Infrared Proximity Sensor

What is the sensitivity of this sensor? For example does it return voltage increments that can be read as 10cm,11cm,12cm, etc. I need a range sensor with a 1 cm resolution between 10 and 20cm for use with a Fez Spider kit via an eblock module.

Th
https://www.seeedstudio.com/Grove---80cm-Infrared-Proximity-Sensor-p-788.html

Jay WilliamsOct 19,2016 19:56 PMAdd Comment

Comment

Popular Topics