Product FAQcarmotor4wdmechanicrobotgear

[FAQ]Ivan asked about L298 Dual H-Bridge Motor Driver

Hi, I want to connect to DC motors with 1.6A stall current each.
Is this driver capable of manage that amount of current or the 2A limit is for the sum of the 2 motors stall current?.


https://www.seeedstudio.com/L298-Dual-H-Bridge-Motor-Driver-p-284.html
Ivan MartinezOct 19,2016 19:49 PMAdd Comment

Comment

Popular Topics