Product FAQbreakoutpcbShieldbreadboardprototypelayoutkitarduinolinkit onekidprototypingbeginner

[FAQ]Guest asked about Protoshield Kit for Arduino

My observations regarding the header alignment. There are two sets of holes used to mount headers. One set (the yellow line in the pic), on both left and right sides of the board, is in the correct position and aligns correctly to plug into the Ard
https://www.seeedstudio.com/Protoshield-Kit-for-Arduino-p-318.html

User name is emptyOct 19,2016 19:49 PMAdd Comment

Comment

Popular Topics