Product FAQmotorpowerdcmechanicalenergy

[FAQ]Christopher Lyons asked about EasyDriver stepper motor driver V4.4

Confused why you say the microstepping mode is permanently set to 8-step. The standard V4.4 board defaults to 8-step mode but this can be changed using pins MS1 or MS2. It appears the board allows access to MS1 & MS2 pins, so why do you say it is perma
https://www.seeedstudio.com/EasyDriver-stepper-motor-driver-V4.4-p-827.html

Christopher LyonsOct 19,2016 19:57 PMAdd Comment

Comment

Popular Topics