Product FAQ

[FAQ]Bryan André asked about CAN-BUS Shield V2

Hi, I have the canbus shield V2 and the canbus shield V1. I am using them to read data from a tire pressure monitor system (including a display). The V1 works great (cs = pin 10, SPI pins = 11, 12 and 13). When I connect the V2 shield I got an error message in the display. I change the pins to make it similar to the V1 shield, but he message continue. I change the pins to obdii standar to can standar, but the message continues. What should I do to make this V2 shield work as the V1 shield?


https://www.seeedstudio.com/CAN-BUS-Shield-V2-p-2921.html
Bryan AndréNov 23,2017 22:21 PMAdd Comment

Comment

Popular Topics